Press Release
Back to Press Room
Quad Port Expander from Diodes Incorporated Provides BoM Savings and Easier PCB Layout for High-Speed Interfaces
Typically, each transceiver requires a dedicated control channel to a host, which is normally implemented using low-speed signal pins and a low-speed protocol, such as I2C and others. As systems become more complex they require more transceivers, putting increased pressure on the host controller to support many more I2C interfaces and other low-speed signal pins.
Using the PI7C1401, four low-speed ports can be aggregated into a single channel and, by combining multiple quad port expanders, a host processor can control up to 56 transceivers through a single I2C/SPI interface. This can significantly lower the pin-count on the host processor or FPGA used to control the high-speed transceivers, as well as ease PCB layout and reduce the overall bill-of-materials (BoM).
The I2C interface supports 1MHz fast mode and allows up to 14 PI7C1401 devices to share a single interface. The devices automatically configure their respective addresses by daisy-chaining their control pins. A bus speed of up to 33MHz is supported when using SPI mode, which effectively allows an unlimited number of PI7C1401 devices to share a single SPI interface. In addition to port aggregation, the PI7C1401 provides a number of other useful features, including four user-programmable GPIO, along with two outputs dedicated to driving status LEDs.
The PI7C1401 also supports automatic pre-fetching of user-defined critical data from the modules, as well as customizable data-driven interrupts, the ability to burst read/write the I2C/SPI interfaces, and a broadcast mode that allows all ports to be written to simultaneously. These features greatly increase the efficiency of PI7C1401's port control in highly demanding applications.
The PI7C1401 quad port aggregator also supports separate host-side I/O voltages, from 1.8V to 3.3V. It is available in a 56-ZF (TQFN) package measuring 5mm x 11mm at 0.5mm pitch, allowing it to be surface-mounted to the underside of a PCB and close to the physical interfaces. Further information is available at www.diodes.com.
About
Recent news releases, annual reports and
View source version on businesswire.com: https://www.businesswire.com/news/home/20190326005098/en/
Source:
Company Contact:
Diodes Incorporated
Emily Yang
VP, Worldwide Sales and Marketing
P: 972-987-3900
E: pressinquiries@diodes.com
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com