Press Release
Back to Press Room
60V, 70dB PSRR LDOs from Diodes Incorporated Deliver Industry-Leading Quiescent Current
The devices have an input voltage range spanning from 5V to 60V, which gives them the flexibility to be connected to 5V, 9V, 12V, 24V, and 48V rails. With a quiescent current of just 2µA, which is significantly below that of competing devices, these LDOs present a minimal draw on the battery resources. As a consequence, the operational runtime of equipment that they are integrated into can be extended.
Despite only consuming 2µA of current, the AP7387 series has a high power supply rejection ratio (PSRR) of 70dB at 1kHz, plus a fast line/load transient response which helps mitigate sudden input voltage and load current changes. Both attributes make them well-suited to noise sensitive implementations.
The AP7387 devices are rated at 150mA output current and are available in 3.0V, 3.3V, 3.6V, and 5V fixed output voltage versions with ±2% output tolerance. Current limit, short-circuit and thermal shutdown protection mechanisms have all been incorporated to improve device and system robustness. In addition, they meet 4kV human body model (HBM) electrostatic discharge (ESD) requirements.
The AP7387 series is supplied in SOT23, SOT25, SOT89, and U-DFN2020-6 packages, and available at
About
DIODES is a trademark of
The Diodes logo is a registered trademark of
View source version on businesswire.com: https://www.businesswire.com/news/home/20220323005041/en/
Company Contact:
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
President
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: