PLANO, Texas--(BUSINESS WIRE)--May 19, 2016-- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, analog and mixed-signal semiconductor markets, today announced the 74LVC1G3157. This single-pole, double-throw analog switch is designed for multiplexing digital or analog signals. Its low on-state resistance ensures high integrity when routing audio signals, making this switching solution well-suited for a wide range of advanced consumer electronics from cell phones, tablets and e-readers to personal music players, hand-held games, satellite navigation and other audio equipment.
Featuring an on-state resistance of less than 6Ω when operated with a 5V supply, the 74LVC1G3157 enables the routing of input audio signals and can even support output routing in low-power applications. Its typical off-state leakage current of 20nA provides a high degree of isolation, allowing components such as resistors and capacitors to be switched in or out of the signal path for programmable filters or different gain configurations.
The 74LVC1G3157 is designed for a 1.65V to 5.5V power supply range and can handle signal amplitudes between VCC and ground. The control input can be up to 5.5V regardless of VCC and the control pin includes hysteresis to allow for slower input rise and fall times. The X2-DFN1410 package occupies just 1.4mm2 of board space, allowing designers to use multiple parts to route multiple signals while the 0.5mm lead pitch eases board assembly. This device is also available in SOT363 package.
For further information, visit the Company’s website at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, analog and mixed-signal semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes’ products include diodes, rectifiers, transistors, MOSFETs, protection devices, function-specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors, power management devices, including LED drivers, AC-DC converters and controllers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. Diodes’ corporate headquarters and Americas’ sales office are located in Plano, Texas and Milpitas, California. Design, marketing, and engineering centers are located in Plano; Milpitas; Taipei, Taiwan; Taoyuan City, Taiwan; Zhubei City, Taiwan; Manchester, England; and Neuhaus, Germany. Diodes’ wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with an additional facility located in Shanghai, China. Diodes has assembly and test facilities located in Shanghai, Jinan, Chengdu, and Yangzhou, China, as well as in Hong Kong, Neuhaus and Taipei. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; Shanghai; Shenzhen, China; Seongnam-si, South Korea; and Munich, Germany, with support offices throughout the world.
Recent news releases, annual reports and SEC filings are available at the Company’s website: http://www.diodes.com. Written requests may be sent directly to the Company, or they may be e-mailed to: diodes-fin@diodes.com.
View source version on businesswire.com: http://www.businesswire.com/news/home/20160519005101/en/
Source: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
972-987-3900
pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
949-224-3874
lsievers@sheltongroup.com