PLANO, Texas--(BUSINESS WIRE)--Jan. 6, 2016-- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today introduced the AP9214L. This device provides single-chip protection for 1-cell lithium-ion (Li+) and lithium-polymer batteries, and is specifically designed for use in rechargeable Li+ battery packs, as found in smart phones, cameras and similar portable electronic equipment. Targeted at the manufacturers of battery protection modules, the device’s accurate monitoring capability delivers safe charging and discharging, prolonging cell lifetime and minimizing energy losses.
The AP9214L co-packages a Li+ protection circuit with a dual N-channel, common-drain MOSFET that can be rapidly turned off when overcharge voltage/current, over-discharge voltage/current, or load short-circuit conditions are detected. A stable temperature-coefficient characteristic contributes to the device’s high-accuracy voltage-detection capability, which can be precisely set within various voltage ranges as required by the end-application. The AP9214L also integrates a built-in fixed detection delay time to reduce external component count.
With a low quiescent current, 3.0µA at +25°C in normal mode (typ), and a MOSFET that boasts an ultra-low RSS(ON) of 13.5mΩ (typ), the AP9214L offers significant power-saving benefits. A power-down mode further cuts the quiescent current to below 0.1µA. The high-voltage CMOS process used to fabricate this device also means it can endure voltage surges up to 30V. An ultra-low profile DFN2535-6 package, with a maximum height of 0.6mm, allows the AP9214L to be used in slim battery-protection modules. Further information is available at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, AC-DC converters and controllers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. Diodes’ corporate headquarters and Americas' sales office are located in Plano, Texas. Design, marketing, and engineering centers are located in Plano; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. Diodes’ wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two additional facilities located in Shanghai, China. Diodes has assembly and test facilities located in Shanghai and in Chengdu, China, as well as in Neuhaus and in Taipei. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; Shanghai; Shenzhen, China; Seongnam-si, South Korea; and Munich, Germany, with support offices throughout the world. For further information, including SEC filings, visit Diodes’ website at www.diodes.com.
View source version on businesswire.com: http://www.businesswire.com/news/home/20160106005415/en/
Source: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-987-3900
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com