Press Release
Back to Press Room
Diodes, Inc. Announces Launch of PowerDI(TM)323 Product Platform Featuring Increased Miniaturization and Efficiency
WESTLAKE VILLAGE, Calif., July 25, 2006 /PRNewswire-FirstCall via COMTEX News Network/ -- Diodes Incorporated ("Diodes") (Nasdaq: DIOD), a leading manufacturer and supplier of high quality discrete and analog semiconductors, today announced the introduction of its high-current density PowerDI(TM)323 product platform with the release of new Schottky Rectifiers and Zener products. The PowerDI(TM)323 product platform meets the growing demand for portability by providing smaller, more efficient discrete devices.
The PowerDI(TM)323 is among the smallest power packages ever introduced in the power rectifier market. It features a footprint of 2.37mm2 and a profile height of 0.7mm, which is 33% lower than current products. Its flat heat sink provides optimal thermal contact and achieves best-in-class power performance. The internal lead frame of the PowerDI(TM)323 is 150% larger than the standard SOD-323 and enables increased forward conduction current to pass through the die at a lower power consumption rate. Diodes' new PowerDI(TM)323 PD3S Schottky Rectifiers are designed to improve efficiency and enable miniaturization of the DC/DC converters in small portable electronics, such as mobile phones, digital audio players and digital cameras.
"With the release of the new PowerDI(TM)323 product platform, Diodes continues to extend its leadership position as an innovator in the discrete market," commented Mark King, Diodes' Sr. VP of Sales and Marketing. "The introduction of the PowerDI(TM)323 product platform builds on the success of our innovative PowerDI product platform that was initiated with the popular PowerDI(TM)5 and PowerDI(TM)123 product lines. As a result of advance marketing efforts at selected key accounts, we have already received notice of our first PowerDI(TM)323 design win into a next-generation digital audio player platform."
In addition, Diodes has extended the PowerDI(TM)323 platform to the Zener market with the PD3Z284C series. The initial release of 5.1 to 12 Volt Zener devices in this new efficient compact package is just the start, as Diodes prepares to roll out Zener devices in voltages that range from 2.4 up to 36 Volts before the end of 2006.
Diodes, Inc. plans to expand the package platform to include TVS devices as well as additional Schottky products by the end of this year.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD) is a leading manufacturer and supplier of high-quality discrete and analog semiconductor products primarily to the communications, computing, industrial, consumer electronics and automotive markets. The Company's corporate sales, marketing, engineering and logistics headquarters is located in Southern California, with two manufacturing facilities in Shanghai, China, a wafer fabrication plant in Kansas City, Missouri, engineering, sales, warehouse and logistics offices in Taipei, Taiwan and Hong Kong, and sales and support offices throughout the world. Diodes, Inc. recently acquired Anachip Corporation, a fabless analog IC company in Hsinchu Science Park, Taiwan.
Diodes, Inc.'s product focus is on subminiature surface-mount discrete devices, analog power management ICs and Hall-effect sensors all of which are widely used in end-user equipment such as TV/Satellite set top boxes, portable DVD players, datacom devices, ADSL modems, power supplies, medical devices, wireless notebooks, flat panel displays, digital cameras, mobile handsets, DC to DC conversion, Wireless 802.11 LAN access points, brushless DC motor fans, and automotive applications. For further information, including SEC filings, visit the Company's website at http://www.diodes.com.
Safe Harbor Statement Under the Private Securities Litigation Reform Act of 1995: Any statements set forth above that are not historical facts are forward-looking statements that involve risks and uncertainties that could cause actual results to differ materially from those in the forward-looking statements, which may include, but are not limited to, such factors as fluctuations in product demand, the introduction of new products, the Company's ability to maintain customer and vendor relationships, technological advancements, impact of competitive products and pricing, growth in targeted markets, risks of foreign operations, and other information detailed from time to time in the Company's filings with the United States Securities and Exchange Commission.
Contact: Crocker Coulson, President, CCG Investor Relations; 310-231-8600 ext. 103; e-mail: crocker.coulson@ccgir.com or Mark King, Sr. VP, Sales & Marketing, Diodes Incorporated: 805-446-4800.
Recent news releases, annual reports, and SEC filings are available at the Company's website: http://www.diodes.com. Written requests may be sent directly to the Company, or they may be e-mailed to: diodes-fin@diodes.com.
PowerDI is a trademark of Diodes Incorporated.
SOURCE Diodes Incorporated
Mark King, Sr. VP, Sales & Marketing of Diodes Incorporated, +1-805-446-4800; or Crocker Coulson, President of CCG Investor Relations, +1-310-231-8600, ext. 103, crocker.coulson@ccgir.com, for Diodes Incorporated
http://www.prnewswire.com