Press Release
Back to Press Room
Diodes Incorporated Announces Expanded Product Offerings Using PowerDI123 and SOD-523 Compact Performance Packages
WESTLAKE VILLAGE, Calif., May 10, 2005 (BUSINESS WIRE) -- Diodes Incorporated (Nasdaq:DIOD), a leading manufacturer and supplier of high quality discrete semiconductors, today announced the continued expansion of its compact power package PowerDI(TM)123 and its ultra-small SOD-523 package in its ongoing efforts to boost the performance of discrete devices, while reducing size and power consumption.
Following the groundbreaking introduction of the compact power package PowerDI(TM)123, this product line has been expanded to include a series of high voltage Schottky devices, boasting a high forward current rating of 1 Ampere and consisting of three voltages, 60V, 100V & 150V.
The key benefits of these new high voltage devices include a low forward voltage drop, high junction temperature rating, and low leakage current. The higher efficiency achievable with PowerDI(TM)123 results in less power loss and longer battery life for portable electronics. As a result, the devices are a superior alternative to the traditional ultra-fast rectifiers typically used in battery chargers, SMPS and consumer electronics applications. Qualified to the AEC-Q101 Standard for High Reliability, they are built with green molding compound and are RoHS compliant, making them also marketable in environmentally conscious overseas markets. Like other products in the PowerDI(TM)123 compact power package, the high voltage series features a footprint of only 6.75mm(2) and a low-profile maximum height of 1mm, thus occupying up to 50% less board space than competitive packages and making them ideal for high integration rectifier applications.
With the release of the new BZT52C5V6T-BZT52C24T zener series, the Company is extending its SOD-523 product line that currently includes Schottky and Switching diodes. The new zener series offers a range of widely-used zener voltages, from 5.6V up to 24V. The height of the ultra-small low profile SOD-523 package is 50% that of the legacy SOD-123 device and occupies less than 25% board space, making the SOD-523 package easier to integrate into space-restricted consumer appliances. All devices are constructed with the environmentally friendly 100% matte tin lead-free plating with green molding compound, qualifying the series as RoHS compliant. The series will be further expanded to include zener voltages below 5.6V and above 24V at a later stage.
"These new additions to our PowerDI(TM)123 and SOD-523 package product lines are yet another fine example of Diodes' flexibility to swiftly extend our performance packages to meet market needs. The high voltage PowerDI(TM)123 product line expansion is our prompt answer to demands for an alternative to ultra-fast rectifiers to extend product longevity. And our new SOD-523 zener series demonstrates Diodes' continued focus on miniaturization in markets where consumer applications constantly shrink in size and weight, and call for increasingly smaller devices that surpass the performance of legacy devices," said Mark King, Vice President of Sales and Marketing for Diodes, Inc.
Product samples are available and in stock now.
For more information, visit http://www.diodes.com or contact Diodes' customer service at 805-446-4800 or email at info@diodes.com.
PowerDI is a trademark of Diodes Incorporated.
About Diodes Incorporated
Diodes Incorporated (Nasdaq:DIOD) is a leading manufacturer and supplier of high-quality discrete semiconductor products, serving the communications, computer, industrial, consumer electronics and automotive markets. The Company operates three Far East subsidiaries, Diodes-China (QS-9000 and ISO-14001 certified) in Shanghai, Diodes-Taiwan (ISO-9000 certified) in Taipei, and Diodes-Hong Kong. Diodes-China's manufacturing focus is on subminiature surface-mount devices destined for wireless devices, notebook, flat panel display, digital camera, mobile handset, set top box, DC to DC conversion, and automotive applications, among others. Diodes-Taiwan is our Asia-Pacific sales, logistics and distribution center. Diodes-Hong Kong covers sales warehouse and logistics functions. The Company's 5" wafer foundry, Diodes-FabTech (QS-9000 certified), specializes in Schottky products and is located just outside Kansas City, Missouri. The Company's ISO-9000 corporate sales, marketing, engineering and logistics headquarters is located in Southern California. For further information, visit the Company's website at http://www.diodes.com.
Safe Harbor Statement Under the Private Securities Litigation Reform Act of 1995: Any statements set forth above that are not historical facts are forward-looking statements that involve risks and uncertainties that could cause actual results to differ materially from those in the forward-looking statements. Potential risks and uncertainties include, but are not limited to, such factors as fluctuations in product demand, the introduction of new products, the Company's ability to maintain customer and vendor relationships, technological advancements, impact of competitive products and pricing, growth in targeted markets, risks of foreign operations, and other information detailed from time to time in the Company's filings with the United States Securities and Exchange Commission.
Recent news releases, annual reports, and SEC filings are available at the Company's website: http://www.diodes.com. Written requests may be sent directly to the Company, or they may be e-mailed to: diodes-fin@diodes.com.
SOURCE: Diodes Incorporated
Diodes Incorporated Mark King, 805-446-4800 or CCG Investor Relations and Strategic Communications Crocker Coulson, 818-789-0100 crocker.coulson@ccgir.com