Press Release
Back to Press Room
Diodes Incorporated Announces High Efficiency Schottky Barrier Rectifiers in Compact PowerDI5 Package; PDS1040 and PDS1040CTL Offer Unparalleled Efficiency and Performance
WESTLAKE VILLAGE, Calif.--(BUSINESS WIRE)--Feb. 2, 2005-- Release of four additional PowerDI(TM)5 Schottky barrier rectifiers fills out product line
Diodes Incorporated, (Nasdaq:DIOD) a leading manufacturer and supplier of high quality discrete semiconductors, today announced the release of two new Schottky barrier rectifiers that offer unparalleled efficiency and performance. These performance products combine lower forward voltage drop with exceptionally low reverse leakage current, resulting in the highest efficiency rectifiers of their type currently available. Packaged in Diodes' thermally efficient low-profile patent-pending PowerDI(TM)5 package, these devices consume only a fraction of the PC board space occupied by competing packages.
"This family of high-efficiency Schottky rectifiers rounds out our portfolio of performance devices employing Diodes' breakthrough PowerDI(TM)5 package, and builds on the momentum that the recent introduction of the 100V and 200V devices generated," said Diodes' President and CEO, C.H. Chen. "Diodes' customer-driven R&D program continues to deliver products that extend the envelope of discrete device performance, while simultaneously consuming less space and power, so as to meet the demands of our global customer base."
The PDS1040 is up to 67% more efficient than competitive packages, and PDS1040CTL up to 79% more efficient, for 50% duty cycle switch-mode operation at an ambient temperature of 125 degrees C, as is commonly found in switch-mode power applications. The switch-mode power supply (SMPS) market is so competitive that even a fraction of a percent improvement in overall final product efficiency is coveted and can make-or-break an SMPS product's marketability.
These silicon-chip level features are enhanced by the benefits of Diodes' patent-pending PowerDI(TM)5 package. With a footprint of only 23.8mm2 and a profile of only 1.1mm, the PowerDI(TM)5 package offers a 65% reduction in PCB real estate as compared to the DPAK package or an 87% reduction as compared to the D2PAK package, making them ideal for space and height limited applications.
Diodes, Inc. is simultaneously releasing four other PowerDI(TM)5 products. The PDS835L and PDS1040L are low forward voltage drop Schottky barrier rectifiers, specifically designed to provide exceptional efficiency in high duty cycle and heavy load applications. The PDS3100 and PDS5100 Schottky barrier rectifiers are ideally suited for high voltage applications.
"While the previously introduced 100V and 200V devices answered the needs of a specific market, our expanded range of Schottky barrier rectifiers offers performance advantages for a wide range of demanding end-equipment applications in the automotive, computing, telecommunications and industrial markets," commented Mark King, Vice President of Sales and Marketing. "Based on the dramatic improvements in size, performance and efficiency, we expect to see strong demand for these devices in power supplies, servers, DC-DC converters, and broad-based automotive applications."
Diodes, Inc. has developed the entire PowerDI(TM)5 product family maintaining the Company's commitment to manufacturing environmentally-conscious products. Featuring "green" Antimony and Bromine-free mold compound and Pb-Free 100% matte Tin plating, these products are RoHS compliant.
Schottky barrier parts are in stock and available for delivery. For a complete product list, visit the Company's website at www.diodes.com.
For more information, visit http://www.diodes.com or contact Diodes' customer service at 805-446-4800 or email at info@diodes.com.
PowerDI is a trademark of Diodes Incorporated. About Diodes Incorporated
Diodes Incorporated (Nasdaq:DIOD) is a leading manufacturer and supplier of high-quality discrete semiconductor products, serving the communications, computer, industrial, consumer electronics and automotive markets. The Company operates three Far East subsidiaries, Diodes-China (QS-9000 and ISO-14001 certified) in Shanghai, Diodes-Taiwan (ISO-9000 certified) in Taipei, and Diodes-Hong Kong. Diodes-China's manufacturing focus is on subminiature surface-mount devices destined for wireless devices, notebook, flat panel display, digital camera, mobile handset, set top box, DC-to-DC conversion and automotive applications, among others. Diodes-Taiwan is our Asia-Pacific sales, logistics and distribution center. Diodes-Hong Kong covers sales warehouse and logistics functions. The Company's 5" wafer foundry, Diodes-FabTech (QS-9000 certified), specializes in Schottky products and is located just outside Kansas City, Mo. The Company's ISO-9000 corporate sales, marketing, engineering and logistics headquarters is located in Southern California. For further information, visit the Company's website at http://www.diodes.com.
Safe Harbor Statement Under the Private Securities Litigation Reform Act of 1995: Any statements set forth above that are not historical facts are forward-looking statements that involve risks and uncertainties that could cause actual results to differ materially from those in the forward-looking statements. Potential risks and uncertainties include, but are not limited to, such factors as fluctuations in product demand, the introduction of new products, the Company's ability to maintain customer and vendor relationships, technological advancements, impact of competitive products and pricing, growth in targeted markets, risks of foreign operations, and other information detailed from time to time in the Company's filings with the United States Securities and Exchange Commission.
Recent news releases, annual reports, and SEC filings are available at the Company's website: http://www.diodes.com. Written requests may be sent directly to the Company, or they may be e-mailed to: diodes-fin@diodes.com.
CONTACT: Diodes Incorporated Mark King, 805-446-4800 or CCG Investor Relations Crocker Coulson, 818-789-0100 crocker.coulson@ccgir.com SOURCE: Diodes Incorporated