Press Release
Back to Press Room
Diodes Incorporated Announces High-voltage Dual-input Charger for
More Reliable Battery Charging
More Reliable Battery Charging
DALLAS, May 19, 2010 (BUSINESS WIRE) --Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets, today announced the release of its API9221 lithium ion/polymer battery charger IC for a variety of handheld equipment requiring both USB and AC/DC power adapter charging inputs. This dual-input IC enables USB host and DC adaptor connections, delivering charge currents in accordance with the USB standard or up to 1.2A, respectively.
To ensure equipment can support a wide range of OEM and aftermarket chargers, the API9221 inputs can withstand a maximum voltage of 28V, which reduces external protection component requirements. To protect the IC, battery, and system, the charger will suspend charging when the input voltage exceeds 5.4V on the USB input or 6.9V on the DC adaptor input. The IC outputs also feature reverse current protection.
The API9221 features a bypass LDO regulator, enabling a host controller to detect the connection of an out-of-specification supply voltage and safely keep the charger in its off-state condition until a valid supply is connected. The device offers excellent thermal regulation and protection, with the ability to reduce charge current to keep the die temperature within safe operating conditions.
The API9221 follows the industry-standard CC/CV charging algorithm, and enables USB and adaptor charge currents and end-of-charge currents to be user-configured via external resistor settings. With only a 1% error across the device's operating temperature range, the IC ensures battery charging up to 4.2V. Further information is available on the Company's website at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, amplifiers and comparators, Hall-effect sensors and temperature sensors, power management devices including LED drivers, DC-DC switching regulators, linear voltage regulators and voltage references along with special function devices including USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters and logistics office are located in Dallas, Texas. A sales, marketing, and engineering office is located in Westlake Village, California. Design centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at http://www.diodes.com.
SOURCE: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-385-2810
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com