Diodes Menu Close

Press Releases

Press Release

Back to Press Room

Diodes Incorporated Announces LDOs that Achieve 2% Accuracy Over Industrial Temperatures

Jul 8, 2010

DALLAS, Jul 08, 2010 (BUSINESS WIRE) --

Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today has introduced a pair of low dropout linear regulators with industrial temperature ratings of -40oC to +85oC. Designed for applications such as set-top boxes, routers, and LCD monitors, the 300mA, 150mV dropout AP7335 and the 600mA, 300mV dropout AP7365 offer adjustable and fixed output voltage operations at an accuracy of 2% across the temperature range.

Input voltage is wide, at 2V to 6V, and both LDOs are capable of delivering an adjustable output voltage between 0.8V and 5.0V and fixed voltages of 0.8V, 1.0V, 1.2V, 1.5V, 1.8V, 2.0V, 2.5V, 2.8V, 3.0V, 3.3V, and 3.9V. Their very low quiescent current of just 35uA means the devices offer power saving benefits in low-power and battery-operated products.

The regulators' ability to drive low ESR 1uF MLCC output capacitors helps to improve stability and reduce circuit cost, while a high PSRR rating of 65db at 1KHz ensures low-noise high-quality supplies for audio and RF applications. LDO robustness is assured by integral over-current, over-temperature, and short-circuit protection.

The LDOs are provided in a choice of industry standard packages and pin-outs, with both devices available in the SOT25 and DFN2020-6 outlines and the AP7365 also available in SOT89-3L and SOT223-3L options. For more information, visit the Company's website at http://www.diodes.com.

About Diodes Incorporated

Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters, logistics center, and Americas' sales office are located in Dallas, Texas. Design, marketing, and engineering centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at http://www.diodes.com.

SOURCE: Diodes Incorporated

Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-385-2810
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com