Press Release
Back to Press Room
Diodes Incorporated Announces a Versatile LED Driver that Increases
Reliability of High Brightness Lamp Systems
Reliability of High Brightness Lamp Systems
DALLAS, May 27, 2010 (BUSINESS WIRE) --Diodes Incorporated (Nasdaq:DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets, today announces a multi-topology LED driver IC designed to increase the reliability of high brightness lamps in automotive, industrial, and commercial lighting systems. The ZXLD1370 LED driver controller operates in buck, boost, and buck-boost modes. It combines patent pending control loops and high-side current sensing to ensure accurate current control of LED strings.
With an extended 6V to 60V operating input voltage range and a typical 1% output current tolerance in all topologies, the driver is capable of delivering the high current levels and tight inter-lamp luminance-matching required by high brightness LED systems. LED reliability and longevity is improved by active LED thermal management achieved via a dedicated external thermistor input, and by fault diagnosis outputs that report the status of LED driver and load.
The ZXLD1370 LED driver controller, used with an external MOSFET, provides a single driver solution capable of supporting a very wide range of LED configurations and current requirements. It supports high accuracy dimming through DC dimming and PWM dimming options. With a dedicated PWM input, the driver offers a 1000:1 dynamic dimming range at 1 kHz. This allows for high accuracy control of color mixing and excellent resolution at low brightness levels.
The device's 1 MHz switching frequency capability with 100 kHz low frequency clamp also means a reduction in the size of the external inductor and simpler design of input EMI filters should they be required. Further information is available on the Company's website at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, amplifiers and comparators, Hall-effect sensors and temperature sensors, power management devices including LED drivers, DC-DC switching regulators, linear voltage regulators and voltage references along with special function devices including USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters and logistics office are located in Dallas, Texas. A sales, marketing, and engineering office is located in Westlake Village, California. Design centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at http://www.diodes.com.
SOURCE: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-385-2810
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com