Press Release
Back to Press Room
Diodes Incorporated Introduces Industry Smallest Bridge Rectifier for Power-Over-Ethernet Applications
DALLAS--(BUSINESS WIRE)--Oct. 28, 2008--Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets, today announced the first in a series of small signal SBR(R) bridge rectifiers, targeting Power-over-Ethernet (PoE) and LED lighting applications. The SBR05M100BLP is the industry's smallest 0.5 Amp bridge in a 3.0mm x 3.0mm leadless package, providing high power dissipation in the smallest footprint available for end-user applications such as Internet Protocol (IP) phones, routers, and LED lighting equipment.
The SBR05M100BLP integrates four highly efficient SBR(R) diodes into one single package, eliminating the need to use four separate individual packages in a bridge configuration. It features a tiny footprint of 9mm2 total physical area, which is 52% smaller in total dimension area and uses 67% less board space than other standard traditional packages such as the HD-DIP case. The SBR05M100BLP also features a very low profile height of 0.6mm, making it ideal for continual reduction of thinner and more portable applications.
The SBR05M100BLP is used in applications requiring a full wave bridge rectifier to convert low voltage AC power signal to a usable DC signal for power devices. It offers a low typical forward voltage drop (VF) of 0.67V at 0.5A rated current at 25 degree C, providing additional power savings for today's energy efficient devices. In a standard application like a PoE device, the AC signal is directly supplied from the RJ45 Ethernet cable and is rectified through a bridge rectifier to a DC signal that can be used to power the device. This eliminates the need for bulky external power supply or adapter to power up the PoE device.
The SBR05M100BLP achieves a continuous forward current up to 0.5A with ultra-low reverse leakage and a high forward surge capability for improved reliability. The new SBR(R) bridge rectifier is rated from an operating temperature of -55 degree C to 150 degree C. Versions of the SBR(R) bridge rectifiers at 40V and 60V are currently in development and will be introduced later this year.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), an S&P SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets, serving the consumer electronics, computing, communications, industrial and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, amplifiers and comparators, Hall-effect sensors and temperature sensors, power management devices including LED drivers, DC-DC switching regulators, linear voltage regulators and voltage references along with special function devices including USB power switch, load switch, voltage supervisor and motor controllers. The Company's corporate headquarters are located in Dallas, Texas. A sales, marketing, engineering and logistics office is located in Westlake Village, California. Design centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, England; with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse and logistics offices are located in Taipei; Hong Kong; Manchester and Munich, Germany, with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at http://www.diodes.com.
CONTACT: Company Contact: Diodes Incorporated John Chiem, 805-446-4800 ext.118 Technical Marketing Engineer john_chiem@diodes.com or Investor Relations Contact: Shelton Group Leanne K. Sievers, 949-224-3874 EVP, Investor Relations lsievers@sheltongroup.com SOURCE: Diodes Incorporated