Press Release
Back to Press Room
Diodes Incorporated Introduces LED Driver that Delivers Higher Current for Low Voltage LED Lamps
DALLAS, Mar 31, 2011 (BUSINESS WIRE) -- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today announced the release of the AL8806 buck LED driver, capable of producing a constant current of up to 1.5A from voltage sources of between 6V and 30V. Suiting MR16, 12V and 24V LED lamp design, the driver ensures a 5% average LED current accuracy for up to 9 high power LEDs over the wide operating voltage range, helping to significantly improve inter-lamp luminance matching.
The high current handling of the AL8806 means it will also meet the needs of the latest multi-die package LEDs, where current levels above 1A are required. This simple, cost-effective driver is packaged in the small footprint low thermal impedance MSOP-8EP, supporting higher LED current drive at higher ambient operating temperatures. Device efficiency is high at up to 98%.
With its maximum output current simply set via a resistor and switching at a frequency of up to 1MHz, the driver helps reduce the size of supporting external components, enabling PCB size to be minimized. Lamp dimming is achieved by applying either a DC voltage or PWM signal that provides a wide range of brightness control that does not overdrive the LED current. For more information, visit the Company's website at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters, logistics center, and Americas' sales office are located in Dallas, Texas. Design, marketing, and engineering centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at www.diodes.com.
SOURCE: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-385-2810
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com