DALLAS--(BUSINESS WIRE)--Nov. 11, 2009--
Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and
supplier of high-quality application specific standard products within
the broad discrete and analog semiconductor markets, has introduced a
pair of N-channel MOSFETs, offering designers of Voice over Internet
Protocol (VoIP) communications equipment a more rugged solution that
significantly reduces circuit complexity and cost.
The ZXMN15A27K and ZXMN20B28K are specifically designed to meet the
stringent requirements of the primary switch position in transformer
based Subscriber Line Interface Circuits (SLIC) with DC/DC converters in
a variety of VoIP applications, including voice over broadband systems,
PBX systems, Cable and DSL gateways.
These devices feature breakdown voltages (BVDSS) of 150V and
200V, respectively, and will withstand the high pulse avalanche energy
and commutation modes in the SLIC environment without the need for
additional protection circuitry. Combined with the right choice of
transformer, these MOSFETs are capable of driving line voltages beyond
150V and supplying multiple subscriber lines at loop lengths exceeding
6km.
The low input capacitance of these MOSFETs makes them easy to drive
directly from the SLIC controlled IC with minimal or no buffering,
further simplifying circuit design and reducing component count and
cost. The ZXMN20B28K is also capable of low gate drive at logic level.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard & Poor’s SmallCap 600 and
Russell 3000 Index company, is a leading global manufacturer and
supplier of high-quality application specific standard products within
the broad discrete and analog semiconductor markets, serving the
consumer electronics, computing, communications, industrial and
automotive markets. Diodes' products include diodes, rectifiers,
transistors, MOSFETs, protection devices, functional specific arrays,
amplifiers and comparators, Hall-effect sensors and temperature sensors,
power management devices including LED drivers, DC-DC switching
regulators, linear voltage regulators and voltage references, along with
special function devices including USB power switch, load switch,
voltage supervisor and motor controllers. The Company’s corporate
headquarters is located in Dallas, Texas. A sales, marketing,
engineering and logistics office is located in Westlake Village,
California. Design centers are located in Dallas; San Jose, California;
Taipei, Taiwan; Manchester, England and Neuhaus, Germany. The Company’s
wafer fabrication facilities are located in Kansas City, Missouri and
Manchester; with two manufacturing facilities located in Shanghai,
China, another in Neuhaus, and a joint venture facility located in
Chengdu, China. Additional engineering, sales, warehouse and logistics
offices are located in Taipei; Hong Kong; Manchester and Munich,
Germany, with support offices located throughout the world. For further
information, including SEC filings, visit the Company's website at http://www.diodes.com.
Source: Diodes Incorporated
Company Contact:
Diodes Incorporated
Francis Tang
VP,
Product Development
P: 972-385-2810
E: pressinquiries@diodes.com
or
Investor
Contact:
Shelton Group
Leanne K. Sievers
EVP,
Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com