DALLAS--(BUSINESS WIRE)--Jul. 7, 2009--
Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and
supplier of high-quality application specific standard products within
the broad discrete and analog semiconductor markets, has introduced a
new family of three low voltage rail-to-rail output operational
amplifiers (op amps), providing a cost effective and small form factor
solution for industrial and consumer electronics.
The LMV321/358/324 op amps operate over the 2.7V to 5.5V supply range,
making them ideal for single supply applications used in set-top-boxes,
computers, data communications, HVAC and other industrial applications
operating from 5V rails. The rail-to-rail output swing increases the
useable supply voltage over the ubiquitous LM358/324, and a smaller
footprint makes them better suited for modern electronic systems.
The LMV321 is provided in SOT23-5 and SOT353 (or SC70-5); the LMV358 is
available in SO8 and MSOP8; and the LMV324 is available in TSSOP14. All
products are offered in green molding compound (no Br and Sb). The
devices have industry standard pin-outs, expanding Diodes’ presence in
industry standard analog. The devices’ operating ambient temperature
range is from -40 to 85oC. The LMV32x family is available
through the Diodes, Inc. distribution channels.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard & Poor’s SmallCap 600 and
Russell 3000 Index company, is a leading global manufacturer and
supplier of high-quality application specific standard products within
the broad discrete and analog semiconductor markets, serving the
consumer electronics, computing, communications, industrial and
automotive markets. Diodes' products include diodes, rectifiers,
transistors, MOSFETs, protection devices, functional specific arrays,
amplifiers and comparators, Hall-effect sensors and temperature sensors,
power management devices including LED drivers, DC-DC switching
regulators, linear voltage regulators and voltage references, along with
special function devices including USB power switch, load switch,
voltage supervisor and motor controllers. The Company’s corporate
headquarters are located in Dallas, Texas. A sales, marketing,
engineering and logistics office is located in Westlake Village,
California. Design centers are located in Dallas; San Jose, California;
Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company’s
wafer fabrication facilities are located in Kansas City, Missouri, and
Manchester; with two manufacturing facilities located in Shanghai,
China, another in Neuhaus, and a joint venture facility located in
Chengdu, China. Additional engineering, sales, warehouse and logistics
offices are located in Taipei; Hong Kong; Manchester; and Munich,
Germany, with support offices located throughout the world. For further
information, including SEC filings, visit the Company's website at http://www.diodes.com.
Source: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP,
Worldwide Analog Products
P: 972-385-2810
E: pressinquiries@diodes.com
or
Investor
Contact:
Shelton Group
Leanne K. Sievers
EVP,
Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com