Press Release
Back to Press Room
Diodes Incorporated's Regulators Raise Efficiency of Low Power System
PLANO, Texas, May 13, 2011 (BUSINESS WIRE) -- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today announced the release of the ZXRE250 and ZXRE252 programmable shunt regulators. These devices feature a very low minimum cathode current for regulation of only 40uA, enabling improved efficiency in a range of applications including power supplies for consumer electronics such as computers, set top boxes and LCD TVs.
With the same electrical specifications as the industry standard TL431 but with a 10x lower cathode current, the three terminal regulators offer excellent temperature stability and output current handling up to 100mA. The devices' regulated output can be set to any voltage between 2.5V and 36V using a pair of external divider resistors.
The ZXRE250 is provided in a choice of SOT23 and SOT25 packages, while the ZXRE252 offers an alternative pinout in SOT23. The parts offer standard reference voltage tolerance options of 1% and 0.5%, with a wide operating temperature range of -40 to 125°C. The regulators can also be used as direct replacements for Zener diodes in applications requiring an improvement in Zener performance. For more information, visit the Company's website at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters, logistics center, and Americas' sales office are located in Plano, Texas. Design, marketing, and engineering centers are located in Plano; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at www.diodes.com.
SOURCE: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-987-3900
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com