Press Release
Back to Press Room
Industry's First DisplayPort 2.0 Active Switch Introduced by Diodes Incorporated
DisplayPort was developed to provide data transfer of high-resolution digital video with audio. Version 2.0 of the DisplayPort specification covers three data rates: 10Gbps (UHBR10), 13.5Gbps (UHBR13.5), and 20Gbps (UHBR20). The PI3DPX8121 is currently the only product that supports the base speed of 10Gbps and includes the multiplexing function noted in the specification.
DisplayPort 2.0 increases the available bandwidth compared with DisplayPort 1.4, which has a maximum data rate of 8.1Gbps per lane. A major advantage of higher bandwidth is that it mitigates the need for data compression, leading to faster systems overall. New consumer products featuring DisplayPort 2.0 are expected by early 2021 and the PI3DPX8121 is poised to help manufacturers meet that 10Gbps (UHBR10) target. .
The PI3DPX8121 ReDriver is compatible with both DisplayPort 1.4 and 2.0 (UHBR10), making it future-resilient. The device also offers protocol agnostic operation, supporting LTTPR (Link Training Transparent PHY Repeater) redrive data path type.
The device integrates CTLE equalizers at the inputs to reduce ISI jitter and compensate for channel loss. PI3DPX8121 also offers programmable flat gain and linearity adjustments.
The PI3DPX8121 is available now, priced at
DisplayPort™ is a trademark owned by the
ReDriver™ is a trademark of
About
View source version on businesswire.com: https://www.businesswire.com/news/home/20200415005054/en/
Company Contact:
VP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: