Press Release
Back to Press Room
Low Standby Power, Non-Isolated Offline Switcher from Diodes Incorporated Significantly Reduces BOM Costs
The AP3928 has a 600mA maximum output current that allows for a 10W output power rating. A key differentiator of this high-voltage switcher IC is that it supports conventional offline non-isolated flyback configurations, as well as more streamlined non-isolated buck configurations, keeping the bill-of-materials (BOM) spend to a minimum.
The peak current and switching frequency will continuously reduce as the load decreases, meaning that this device can achieve heightened degrees of efficiency in light load conditions. It is thereby well-suited for any form of equipment that spends prolonged time in sleep mode.
The AP3928’s low standby power of less than 30mW is another important attribute. This is of particular value in small domestic appliances and IoT devices, where available battery power needs to be conserved.
The DIODES AP3928 switcher IC is supplied in a compact SO-8 package. To ensure safety, it meets high-voltage creepage requirements, and can support operational junction temperatures reaching up to +150°C. Overtemperature, output short, overload and open-loop protection functions are all included, as well as undervoltage lockout. The AP3928 is available at
DIODES is a trademark of
The DIODES logo is a registered trademark of
About
View source version on businesswire.com: https://www.businesswire.com/news/home/20220208005022/en/
Company Contact:
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
President
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: