Diodes Menu Close

Press Releases

Press Release

Back to Press Room

Precision Op Amp from Diodes Incorporated Features Ultra-Low Input Offset Voltage and Low Noise

Jul 30, 2020

PLANO, Texas--(BUSINESS WIRE)--Jul. 30, 2020-- Diodes Incorporated (NASDAQ: DIOD) today announced its first precision operational amplifier. The AS2333 uses chopper stabilization to achieve ultra-low input offset voltage of 8µV (typical) and near-zero drift (0.02µV/degree C, typical) over time and temperature. The chopper stabilization also addresses low frequency 1/f noise and offset voltage crossover distortion. Typical applications for the AS2333 include transducers, medical equipment, chemical detectors, and handheld test instruments.

The AS2333 features a typical common-mode rejection ratio of 120dB and a typical open loop gain of 130dB useful for small signal sensors that measure parameters such as pressure, sound, light, temperature, voltage, and current. As many applications have very low output signals, they require precision amplification with low offset and low noise.

The high precision, dual channel amplifier also features high impedance inputs with a common-mode range 100mV beyond the supplies and an output swing that is within 50mV of the rails. Features for battery-operated applications include a typical quiescent current of 12μA and supplies as low as 1.8V (±0.9V).

The AS2333 is available in SO-8 and MSOP-8 packages priced at $0.38 in 2500 piece quantities.

About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the consumer electronics, computing, communications, industrial, and automotive markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 28 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information, visit www.Diodes.com.

Company Contact:
Diodes Incorporated
Emily Yang
VP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us

Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com

Source: Diodes Incorporated