Press Release
Back to Press Room
ReTimers with Adaptive Equalization and Bidirectional Capabilities from Diodes Incorporated Bring Power-Efficient, Low-Latency Operation to USB-C/DP Designs
The new retimers each feature receiver adaptive equalization, which means that both long trace and short trace applications can be addressed. This function enables channel loss compensation up to -23dB for signal transmissions at 5GHz speeds and -18dB for 4.05GHz speeds plus jitter cleaning, without the need for a local reference clock.
The PI2DPT1021 supports 10Gbps USB3.2 Gen2 and DisplayPort™ (DP) version 1.4, while the PI2DPT821 supports 8.1Gbps DP1.4 and USB3.2 Gen1 protocols. A bidirectional, high-speed channel is incorporated into each device, which allows the flow from downstream facing ports (DFP) and upstream facing ports (UFP) to be swapped. As a result, engineers have greater layout flexibility when it comes to signal flow direction. In particular, thanks to their bidirectional operation, the PI2DPT1021 and PI2DPT821 are suitable for active cable implementations since both of their end connectors are the same and can act as either a DFP or UFP accordingly.
Other key attributes for these latest Diodes’ retimers are an ultra-low latency from signal input to output (<1ns) and a broad temperature range (covering 40°C to +85°C). Both have an I2C programming interface. Automatic power saving modes, applicable to both USB and DP, are pivotal in minimizing energy consumption.
The PI2DPT1021 and PI2DPT821 retimers are supplied in 32-pin QFN packages with 2.85mm x 4.5mm x 0.45mm dimensions. These devices are available at
About
The Diodes logo is a registered trademark of
DIODES™ is a trademark of
All other trademarks are the property of their respective owners.
View source version on businesswire.com: https://www.businesswire.com/news/home/20221208005034/en/
Company Contact:
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
President
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: