PLANO, Texas--(BUSINESS WIRE)--Apr. 23, 2015-- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today introduced a single-channel load switch designed to operate from 4.5V up to 12V with a near-zero quiescent supply current that makes it suitable for use in battery-powered netbooks, tablets and e-Readers. The AP22850 can handle power up/down sequencing with load currents up to 8A and adjustable start-up and discharge rates. It is offered in the space-saving, thermally efficient 2mm x 2mm x 0.8mm W-DFN2020-8 package, maximizing available board space.
The ever-increasing portable-computing market continues to demand more integrated and capable load switches. These are required for distributed power control and low-voltage differential signalling where switches rated for continuous output-current operation with power-good indication and adjustable discharge are key. These functions and performance are delivered cost-effectively by the AP22850, which is based on a P-channel MOSFET that has a low typical RDS(ON) of 20mΩ. The device can handle inputs up to 12V with a maximum output current of 8A but with a quiescent (no-load) current of just 1.2nA.
The AP22850 does not require an external gate pull-up resistor and integrates circuitry to suppress fast input transients from coupling to the output; these features contribute to reduced BOM costs and board area savings. Further information is available at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, AC-DC converters and controllers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. Diodes’ corporate headquarters and Americas' sales office are located in Plano, Texas. Design, marketing, and engineering centers are located in Plano; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. Diodes’ wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two additional facilities located in Shanghai, China. Diodes has assembly and test facilities located in Shanghai and in Chengdu, China, as well as in Neuhaus and Taipei. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; Shanghai; Shenzhen, China; Seongnam-si, South Korea; and Munich, Germany, with support offices throughout the world. For further information, including SEC filings, visit Diodes’ website at www.diodes.com.
Source: Diodes Incorporated
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
972-987-3900
pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
949-224-3874
lsievers@sheltongroup.com