Press Release
Back to Press Room
Three-Level Configurable Slew-Rate Controlled Power Switch from Diodes Incorporated Simplifies and Enhances Power-Rail Management in Solid State Drives
The N-channel MOSFET, with a built-in charge pump inside the AP22980, has an extremely low Rds(ON) of 5.1mΩ enabling loads reaching 6A while minimizing voltage drops and power losses in high current loading applications. By having a separate VBIAS pin, the minimum input voltage that it is capable of supporting is significantly lower, resulting in a wider input voltage range that can be covered - from 0.285V to 5.5V - enabling greater application flexibility.
With 60µA (typical) quiescent supply current, the AP22980 is highly optimized for situations where keeping standby power consumption down is a priority. This device has an operational temperature range of -40°C to 105°C. If the junction temperature exceeds 150°C, an overtemperature protection mechanism is triggered.
The AP22980 three-level selectable slew rate power switches are supplied in the compact W-QFN1520 package that takes up little board space and eases integration. These devices are available at
About
The Diodes logo is a registered trademark of
DIODES™ is a trademark of
All other trademarks are the property of their respective owners.
View source version on businesswire.com: https://www.businesswire.com/news/home/20221216005016/en/
Company Contact:
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
President
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: