Press Release
Back to Press Room
Tunable Linear ReDrivers from Diodes Incorporated Support Superior Levels of Signal Integrity on High-Speed DisplayPort 2.0 and HDMI 2.1 Interfaces
Supporting 13.5Gbps data rates, the 4-lane PI3DPX8112 is applicable to DisplayPort™ 2.0 implementations (as well as earlier generations of the protocol). Alongside this is the 4-lane PI3HDX12212, which has 12Gbps performance capabilities that mean it can manage HDMI 2.1, HDMI 2.0, HDMI 1.2, and HDMI 1.4 transmission modes.
Both the PI3HDX12212 and PI3DPX8112 ReDrivers feature pin strap adjustable 8-level receive equalizer settings on each of their two output paths, plus 4 settings for the adjusting of output flat gain and output swing parameters. Through these adjustments, it is possible for the signal integrity to be tuned in accordance with specific application requirements. Channel losses can then be compensated for and inter-symbol interference (ISI) removed to help extend channel reach. These devices are able to accept lower supply voltages than those achievable by the competition. They are protocol agnostic, transparent to channel link training, and deliver ultra-low latency operation.
The PI3DPX8112 and PI3HDX12212 are both supplied in 32-pin TQFN packages (with 3mm x 6mm dimensions) that are highly suitable for incorporation into space-limited environments. Both devices support a working temperature range of -40°C to +85°C. In 5,000 piece quantities, the PI3DPX8112 has a unit cost of
DisplayPort™ and the DisplayPort™ logo are trademarks owned by the
HDMI, High-Definition Multimedia Interface, and the HDMI logo are trademarks or registered trademarks of
ReDriver™ is a trademark of
About
View source version on businesswire.com: https://www.businesswire.com/news/home/20210729005063/en/
Company Contact:
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: