Press Release
Back to Press Room
USB Type-C PD3.0 Sink Controllers from Diodes Incorporated Enable Streamlined and Cost-Effective Charging Solutions
The AP33771’s simple pin-driven setting of required voltages and power makes it easier to use, while the AP33772 provides greater flexibility for more sophisticated designs that use a µC (with an I2C interface included). Both devices have built-in application firmware, which automatically carries out the PD3.0 negotiation procedure with the attached USB PD3.0 compliant charger in order to obtain the required power level. LED lighting (driven by one of their GPIOs) enables a clear indication of the charging state and potential fault situation.
The AP33771 has a preloaded power menu, consisting of eight different output voltages and 10 different power levels. The power requirements of the end equipment can be met via alteration of simple resistor settings. It also provides 5V charging when connected to a classical USB Type-A charger, as well as supporting USB Type-C to USB Type-C cable voltage drop compensation.
The I2C interface on the AP33772 allows more sophisticated system designs to be addressed. Through it, particular power profiles can be specified, as well as enabling access to various protection features.
The AP33771 and AP33772 are supplied in 24-pin W-QFN4040 packages. They are available at
About
USB Type-C® and USB-C® are registered trademarks of
The Diodes logo is a registered trademark of
DIODES is a trademark of
View source version on businesswire.com: https://www.businesswire.com/news/home/20220609005143/en/
Company Contact:
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
President
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: