Press Release
Back to Press Room
10Gbps Automotive-Compliant Active Crossbar Mux from Diodes Incorporated Simplifies Smart-Cockpit Connectivity
The PI3DPX1225Q supports three operating modes: the device can connect one lane of USB 3.2 Gen 2 to the USB Type-C connector; one lane of USB 3.2 Gen 2 and two channels of DP 2.1 UHBR10; or four channels of DP 2.1 UHBR10. The device also integrates an AUX listener and, in compliance with the USB Type-C standard, swaps the AUX channels when a flipped cable is detected.
For each of the USB 3.2 Gen 2 and DP 2.1 UHBR10 operating modes, the differential signals can be easily adjusted with continuous time linear equalization (CTLE). Output compression swing (-1dB) and flat-gain values are controlled by the I2C setting. By reducing intersymbol interference (ISI) jitter, the 10Gbps signal performance is optimized over a variety of physical mediums. Linear equalization does not block the decision feedback equalizer (DFE) receiver’s adaptive channel controls—this supports DP 2.1 transparent link training (LT) without dependency on the DP-AUX channels listener.
The PI3DPX1225Q is packaged in a 40-Pin W-QFN6040-40 with a compact 4mm x 6mm footprint. The PI3DPX1225Q is available from
About
The Diodes logo is a registered trademark of
* Automotive-compliant—qualified to AEC-Q100 Grade 3, manufactured in facilities certified to IATF 16949, and supports PPAP documents.
ReDriver™ is a trademark of
All other trademarks are the property of their respective owners.
© 2024
View source version on businesswire.com: https://www.businesswire.com/news/home/20240820695553/en/
Director, Investor Relations & Corporate Marketing
+1 408-232-9003
Contact Us
Source: