Press Release
Back to Press Room
20Gbps 2x2 Exchange Switch from Diodes Incorporated Enables Fast Multiplexing/Switching in Automotive Media and Driver Assistance Systems
The automotive-compliant PI3DBS16222Q enables 2x2 differential multiplexing at speeds of 20Gbps, and supports USB 3.2 Gen 2, PCI Express 4.0, and 10GBASE-KR standards. The device leverages a proprietary design technique, enhancing its dynamic electrical characteristics. This delivers low insertion-loss (-2.0dB at 10GHz typical) and crosstalk (-17dB at 10GHz typical) figures, ensuring high signal-integrity levels. In addition, the device attains a 10ps bit-to-bit skew, and a low return-loss.
The PI3DBS16222Q high-speed, multi-channel exchange switch from Diodes is AEC-Q100 Grade 2 qualified, manufactured in IATF 16949 certified facilities, and supports PPAP documentation. It is supplied in a compact 2.5mm x 4.5mm TQFN-30L (ZL30) package, and it is available at
About
The Diodes logo is a registered trademark of
All other trademarks are the property of their respective owners.
© 2023
View source version on businesswire.com: https://www.businesswire.com/news/home/20230316005063/en/
Company Contact:
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
President
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: