Press Release
Back to Press Room
300mA Output Automotive-Compliant LDOs from Diodes Incorporated with Power Good Support Off-Battery Point-of-Load
The power-good indicator output that is featured on each of the AP7583AQ series devices is an important differentiator. This enables ongoing supply monitoring. It also provides fault reporting capabilities and facilitates power sequencing.
The AP7583AQ and AP7583Q devices have fixed output voltage versions (3.3V and 5V), and adjustable output versions. They support a wide input voltage from 3V to 42V. This, in combination with their low-dropout voltage, allows these LDOs to support cold-cranking and handle load dump situations.
The ultra-low quiescent current is another key characteristic of the AP7583AQ and AP7583Q series. This is only 3µA at light loads—making them highly optimized for powering “always-on” components such as the microcontroller units (MCUs) and CAN transceivers in standby systems.
The AP7583AQ and AP7583Q series are AEC-Q100 Grade 1 qualified, manufactured in IATF 16949 certified facilities, and support PPAP documentation. Both LDO series are supplied in 6-pin W-DFN2020 packages. In addition, the AP7583AQ series is offered in 8-pin MSOP and 4-pin TO252 package formats. In 1,000 piece quantities, the AP7583AQ series is available at
About
Automotive-compliant - AEC qualified, manufactured in IATF 16949 certified sites supporting PPAP documents.
The Diodes logo is a registered trademark of
All other trademarks are the property of their respective owners.
© 2023
View source version on businesswire.com: https://www.businesswire.com/news/home/20230914394733/en/
Director, Investor Relations & Corporate Marketing
+1 408-232-9003
Contact Us
Source: