Press Release
Back to Press Room
Diodes Incorporated Announces Power Switches that Provide Complete
USB Port Protection
USB Port Protection
DALLAS, May 13, 2010 (BUSINESS WIRE) --Diodes Incorporated (Nasdaq:DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets, today announced the release of a family of 6 high-side power switches offering complete port protection for a wide range of self-powered and bus-powered USB and other hot swap applications. Designed to tolerate heavy capacitive loads and short circuits, the AP21x2A dual channel devices are available with maximum load current ratings of 0.5A, 1.0A and 1.5A, and both polarities of enable input.
To improve system robustness, the power switches deliver a fast transient response of 2us to prevent spurious shutdown or restart. They provide tight tolerance current limiting at ratings of 0.8A, 1.4A or 2.0A, over-temperature and short-circuit protection as well as controlled rise-time and under-voltage lockout functionality.
The AP21x2A products integrate an automatic output discharge function to provide controlled discharge of disabled output capacitor voltage, and offer improvement in on-resistance over existing dual channel devices. A 7ms deglitch time on the power switch's fault report flag prevents any false over-current reporting and does not require the addition of any external components. The package options with industry standard pin-outs are: SO8, MSOP-8, MSOP-8-EP and DFN3030E-8.
The devices are UL Recognized and IEC 60950-1 CB Scheme Certified to ensure public safety and product quality. Their ambient operating temperature range is -40 to 85oC. Further information is available on the Company's website at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq:DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, amplifiers and comparators, Hall-effect sensors and temperature sensors, power management devices including LED drivers, DC-DC switching regulators, linear voltage regulators and voltage references along with special function devices including USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters and logistics office are located in Dallas, Texas. A sales, marketing, and engineering office is located in Westlake Village, California. Design centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at http://www.diodes.com.
SOURCE: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-385-2810
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com