Press Release
Back to Press Room
Diodes Incorporated Extends Logic Family with Open Drain Parts
DALLAS, Jul 27, 2010 (BUSINESS WIRE) --
Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today announced that it has extended its family of single-gate logic products with the introduction of open drain functions in both standard and enhanced performance versions. Direct replacements for industry standard parts, the devices are suitable for voltage level shifting, active low wired OR, and active high wired AND applications. The 74LVC1G06, 74LVC1G07, 74LVCE1G06 and 74LVCE1G07 parts are available in SOT25 and SOT353 packages.
With a wide operating voltage range of 1.65 to 5.5V, the 74LVC1G06 and 74LVC1G07 will suit both portable battery powered as well as traditional 5V applications, while the 1.4V to 5.5V operating voltage range of the enhanced performance 74LVCE1G06 and 74LVCE1G07 enables them to be used in 1.5V logic systems as well. Applications include cell phones, notebooks, netbooks, TVs, E-readers, personal navigation, and entertainment devices.
Capable of drawing less than 1uA of supply current, Diodes' open drain logic parts ensure energy efficient operation and when the device is powered down, IOFF output circuitry disables the output to prevent backflow current from affecting performance. For more information, visit the Company's website at www.diodes.com/logic.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters, logistics center, and Americas' sales office are located in Dallas, Texas. Design, marketing, and engineering centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at http://www.diodes.com.
SOURCE: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-385-2810
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com