Diodes Incorporated Introduces a Dual MOSFET Combination That Saves Space Without Compromising Performance
DALLAS--(BUSINESS WIRE)--May. 27, 2009--
Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and
supplier of high-quality application specific standard products within
the broad discrete and analog semiconductor markets, today introduced a
complementary pair of 100V enhancement mode MOSFETs in an SO8 package
that achieves the same performance as that of much larger individually
packaged parts. The ZXMC10A816 is aimed at H-bridge circuits in DC fan
and inverter circuits, Class D amplifier output stages, and an array of
48V applications.
Enabling designers to replace equivalent devices in SOT223 and DPak
(TO252) packages, the N- and P-channel MOSFET combination reduces board
space and component count as well as simplifies gate drive circuit
layouts. As an illustration of its space saving potential, the SO8
package’s footprint of just 31mm2 is only 30% that of two
SOT223 MOSFETs.
The N- and P-channel MOSFETs used in the dual device package exhibit low
gate charge and typical RDS(ON) of 230mΩ and 235mΩ,
respectively, at VGS of 10V, ensuring that switching and
on-state losses are minimized. Both 2.4W and 2.6W are respective power
dissipation figures.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard & Poor’s SmallCap 600 and
Russell 3000 Index company, is a leading global manufacturer and
supplier of high-quality application specific standard products within
the broad discrete and analog semiconductor markets, serving the
consumer electronics, computing, communications, industrial and
automotive markets. Diodes' products include diodes, rectifiers,
transistors, MOSFETs, protection devices, functional specific arrays,
amplifiers and comparators, Hall-effect sensors and temperature sensors,
power management devices including LED drivers, DC-DC switching
regulators, linear voltage regulators and voltage references, along with
special function devices including USB power switch, load switch,
voltage supervisor and motor controllers. The Company’s corporate
headquarters are located in Dallas, Texas. A sales, marketing,
engineering and logistics office is located in Westlake Village,
California. Design centers are located in Dallas; San Jose, California;
Taipei, Taiwan; Manchester, England and Neuhaus, Germany. The Company’s
wafer fabrication facilities are located in Kansas City, Missouri and
Manchester; with two manufacturing facilities located in Shanghai,
China, another in Neuhaus, and a joint venture facility located in
Chengdu, China. Additional engineering, sales, warehouse and logistics
offices are located in Taipei; Hong Kong; Manchester and Munich,
Germany, with support offices located throughout the world. For further
information, including SEC filings, visit the Company's website at http://www.diodes.com.
Source: Diodes Incorporated
Company Contact:
Diodes Incorporated
Francis Tang
VP
Product Development
972-385-2810
pressinquiries@diodes.com
or
Investor
Relations Contact:
Shelton Group
Leanne K. Sievers
EVP,
Investor Relations
949-224-3874
lsievers@sheltongroup.com