Press Release
Back to Press Room
Diodes Incorporated Introduces High Frequency Buck Converter to Save Space and Increase Efficiency
DALLAS, Mar 30, 2010 (BUSINESS WIRE) --Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets, today announced the release of its AP5100 step-down converter, which has been designed to bring space savings and efficiency improvements to set-top box, modem and distributed power applications. Provided in the compact 6-pin SOT26 package, this low-cost converter features a built-in power MOSFET and internal compensation to limit external component requirements.
Operating at a fixed switching frequency of 1.4Mhz, the AP5100 also enables a reduction in the overall size of external components, particularly the inductor. With its low series on-resistance power MOSFET switch, the converter is capable of delivering a constant current output of up to 1.2A at 90% efficiency over a wide input supply range, from 4.75V to 24V. The output is adjustable via a resistor divider, from 0.81V to 15V.
The device's current mode operation provides for a fast transient response over the full operating input voltage and temperature range. The AP5100 has an enable pin allowing it to be put into standby mode where it consumes just 0.1uA. The AP5100 is self-protected, featuring on-chip thermal shutdown and cycle-by-cycle over-current protection to help ensure long-term product reliability.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets, serving the consumer electronics, computing, communications, industrial and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, amplifiers and comparators, Hall-effect sensors and temperature sensors, power management devices including LED drivers, DC-DC switching regulators, linear voltage regulators and voltage references, along with special function devices including USB power switch, load switch, voltage supervisor and motor controllers. The Company's corporate headquarters and logistics office are located in Dallas, Texas. A sales, marketing, and engineering office is located in Westlake Village, California. Design centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester; with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse and logistics offices are located in Taipei; Hong Kong; Manchester and Munich, Germany, with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at http://www.diodes.com.
SOURCE: Diodes Incorporated
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
972-385-2810
pressinquiries@diodes.com
or
Investor Relations:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
949-224-3874
lsievers@sheltongroup.com