Press Release
Back to Press Room
Diodes Incorporated Launches Miniature SOT963 Packaged Devices for
Ultra Portable Electronics
Ultra Portable Electronics
DALLAS, Jun 21, 2010 (BUSINESS WIRE) --Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today has introduced bipolar transistor, MOSFET, and TVS devices in the ultra small SOT963 package, achieving the same or better performance of much larger packaged parts.
Suiting low power applications, the SOT963 with its 0.7mm2 footprint is 30% smaller than SOT723 alternatives and 60% smaller than that of SOT563 packages. The footprint savings combine with the SOT963's 0.5mm off-board height to address a wide range of ultra portable electronic product requirements.
The initial SOT963 package portfolio comprises six general-purpose dual bipolar transistor combinations, three small signal dual MOSFET combinations, and a quad transient voltage suppressor array - the DUP412VP5. The devices' leaded package enables hand soldering and visual inspection, removing the need for x-ray inspection.
The dual transistors are offered with VCEO ratings of 40V and 45V and include dual NPN, dual PNP and complementary NPN and PNP pairings. The dual N, dual P and complementary MOSFETs are rated at BVDSS of 20V and have RDS(ON) ratings specified at 1.5V. Further information can be found at the Company's website at http://www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters, logistics center, and Americas' sales office are located in Dallas, Texas. Design, marketing, and engineering centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at http://www.diodes.com.
SOURCE: Diodes Incorporated
Company Contact:
Diodes Incorporated
Francis Tang
VP, Worldwide Discrete Products
P: 972-385-2810
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com