Press Release
Back to Press Room
Diodes Incorporated Releases Its First Silicon Carbide Schottky Barrier Diodes (SBD)
These wide-bandgap SBDs bring the benefits of significantly improved efficiency and high-temperature reliability, while also responding to market demands for reduced system running costs and low maintenance. The devices are suitable for AC-DC, DC-DC, and DC-AC switching converters, photovoltaic inverters, uninterruptable power supplies, and industrial motor drive applications. These devices can also be used in a variety of other circuits, such as boost converters for power factor correction.
The efficient performance of these SiC devices are superior to those of conventional silicon-based products, and provide power supply designers with uncompromising product performance benefits, such as:
- Negligible switching losses due to low capacitive charge (QC) that provide high efficiency in fast switching applications. This is suitable for circuit designs with higher power density and smaller overall solution size.
- Low forward voltage (VF) that further improves efficiency, reducing power losses and operational costs.
- Reduced heat dissipation that helps lower overall system cooling budgets.
- High surge current capability that increases robustness for better system reliability, while excellent thermal performance reduces build costs.
Three package options include surface mount TO252-2 (Type WX), through-hole TO220AC (Type WX), and ITO220AC (Type WX-NC).
The DSCxxA065 and DSCxx120 series are available from
About
The Diodes logo is a registered trademark of
DIODES is a trademark of
All other trademarks are the property of their respective owners.
View source version on businesswire.com: https://www.businesswire.com/news/home/20230130005018/en/
Company Contact:
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
President
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: