Press Release
Back to Press Room
Diodes Incorporated's DC/DC Converters Increase Efficiency
PLANO, Texas, May 05, 2011 (BUSINESS WIRE) -- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today introduced the AP6507 and AP6508 synchronous DC/DC buck converters. Delivering a continuous load current of up to 3A, the AP6507 and AP6508 converters offer designers of distributed power systems an operating efficiency as high as 90%. With input voltage ranges of 4.5V to 18V and 4.5V to 21V respectively, these compact converters will support the needs of low voltage 5V and 12V bus systems in a broad range of consumer electronic products, including monitors, LCD TV and set-top box.
Using a simple external resistor divider, the adjustable output of the DC/DC converters can be set to any voltage down to as low as 0.8V. To meet demands for increased power densities, the converters are provided in space-saving exposed pad package options: the AP6507 in SO-8EP, and the AP6508 in DFN4030-14EP.
By operating at a high switching frequency of 500kHz, the converters can also make use of smaller external components. That smaller footprint along with the devices' integration of high- and low-side MOSFET switches, internal compensation and protection features, enables significant system board space savings.
The integrated overcurrent protection and thermal shutdown features of both DC/DC converters combine to increase system stability and achieve long-term reliability. Additional features provided by the AP6508 are an externally programmable soft-start function and a power good flag, enabling the implementation of power sequencing and ramp control. For further information, visit the Company's website at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters, logistics center, and Americas' sales office are located in Plano, Texas. Design, marketing, and engineering centers are located in Plano; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri, and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at www.diodes.com.
SOURCE: Diodes Incorporated
Diodes Incorporated
Julie Holland, 972-987-3900
VP, Worldwide Analog Products
pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers, 949-224-3874
EVP, Investor Relations
lsievers@sheltongroup.com