Press Release
Back to Press Room
Diodes Incorporated's Low Power Current Monitors Provide Accurate Current Measurement
DALLAS, Mar 16, 2011 (BUSINESS WIRE) -- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today announced the release of the ZXCT11xx series of low power high-side current monitors. With an operating current of only 3uA, the ZXCT11xx series of monitors provides accurate, high efficiency measurement of load current in motor drive, overload protection and safety applications such as computer power adapters, appliance motor controls, and power automotive safety and convenience features.
Coupled with their low operating current performance, the devices' wide common-mode voltage range, of 2.5V to 36V, and their extended -40C to 125C temperature range are well suited to higher supply voltage automotive, industrial and white goods circuit design.
Requiring just a single external gain-setting resistor in addition to a low value sense resistor, the ZXCT11xx monitors are simple to use, keep component count to a minimum and save space with their SOT23 packaging. Sensing current on the high-side also avoids any ground plane disruption.
Offering a range of pin-outs to help optimize board layouts, the ZXCT1107 and ZXCT1109 are 3-pin SOT23 package variants. The ZXCT1110 is a 5-pin device with a separate ground pin facilitating improved performance. For more information, visit the Company's website at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters, logistics center, and Americas' sales office are located in Dallas, Texas. Design, marketing, and engineering centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at www.diodes.com.
SOURCE: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-385-2810
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com