Press Release
Back to Press Room
Diodes Incorporated's Versatile 9-Channel LED Drivers Improve LCD Backlighting Performance with 93% Efficiency and 1% Channel Matching
DALLAS, Sep 28, 2010 (BUSINESS WIRE) -- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today announced two 9-channel LED drivers with internal charge-pumps for backlighting small-LCD screens, keypads and LED lights. Working from 2.7V to 5.5V and driving 20mA, the applications include mobile phones and other portable consumer devices. Driving three groups of 3-LED channels and its three independent PWM dimmable control inputs, the AL3158 provides a simple drive for RGB LEDs. The AL3159, with its versatile 3-wire logic decoding of LED current control, simplifies the driving of 9-LEDs for illuminating LCD screens and LED indicator control.
The inductor-less solution requires only three external capacitors to complete the driver circuit. High levels of functional integration coupled with thin QFN packages mean that these devices save board space and reduce manufacturing costs. The devices offer up to 93% power efficiency, maximize battery life, and feature 1% current matching accuracy between channels to deliver an extremely even, consistent screen image.
LED open and short-circuit protection, thermal and under-voltage lockout and over voltage protection are provided on all channel outputs to maximize reliability. A soft start function reduces power supply inrush current to maximize battery-operating life. Both drivers are available in a lead-free, thermally enhanced, 20-pin 3mm x 3mm 0.6mm height QFN package. For more information, visit the Company's website at http://www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters, logistics center, and Americas' sales office are located in Dallas, Texas. Design, marketing, and engineering centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at http://www.diodes.com.
SOURCE: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-385-2810
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com