Press Release
Back to Press Room
Diodes Incorporated's World's Smallest Hall Effect Switch Saves Power as Well as Space
DALLAS, Apr 13, 2011 (BUSINESS WIRE) -- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today announced the release of the world's smallest dual output omnipolar Hall effect switch IC, specifically designed for open/close detection in portable, battery-powered products including cell phones and notebook PCs. The dual output AH1891 is optimized for operation over the supply voltage range 1.8V to 3.3V and offers a sleep function, assuring an average current consumption of only 7uA.
Provided in an 0.8mm x 0.8mm CSP package, the IC is some 13 times smaller than common 3-leaded TSOT packaged alternatives and is significantly smaller than other DFN and SOT553 packaged parts. The AH1891's PCB space saving advantage is also complemented by a reduction in off-board height, with the IC's profile measuring less than 0.5mm. In addition, the IC's integrated pull-up resistors help simplify the external applications circuit.
Being an omnipolar (north and south pole operated) and dual output device, the AH1891 provides the design flexibility to suit a variety of low power circuit architectures. When a magnetic flux density is detected and exceeds the IC's operating point, output 1 is pulled low while output 2 is inverted high, enabling different logic systems to be accommodated. Output states are held until magnetic flux density is lower than the IC's release point.
With operating and release points optimized and stable over the temperature range -40C to 85C, the AH1891 is immune to the possibility of early or late switching effects. The IC also offers good immunity to RF noise and other circuit stresses. For more information, visit the Company's website at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. The Company's corporate headquarters, logistics center, and Americas' sales office are located in Dallas, Texas. Design, marketing, and engineering centers are located in Dallas; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. The Company's wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two manufacturing facilities located in Shanghai, China, another in Neuhaus, and a joint venture facility located in Chengdu, China. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; and Munich, Germany; with support offices located throughout the world. For further information, including SEC filings, visit the Company's website at www.diodes.com.
SOURCE: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-385-2810
E: pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com