Diodes Incorporated
Investors

Press Releases

Press Release

Back to Press Room

Four-Channel ReDriver™ from Diodes Incorporated Delivers 32Gbps Signal Integrity for Next-Generation Automotive Smart Cockpit Platforms

May 6, 2026

SANTA CLARA, Calif.--(BUSINESS WIRE)--May 6, 2026-- Diodes Incorporated (Diodes) (Nasdaq: DIOD) introduces the PI3EQX32904Q, an automotive-compliant*, 32Gbps, four-channel linear ReDriver that optimizes signal integrity for high-speed protocols such as PCI Express® (PCIe®) 5.0 specification, SAS4, and CXL. Targeting smart cockpit architectures that integrate advanced driver-assistance systems (ADAS), infotainment systems, and instrument clusters into a single unit, the device addresses the growing signal-integrity challenges posed by these AI-driven computing platforms.

Designed for GPU+CPU SoC architectures, the PI3EQX32904Q employs a 0.13µm silicon germanium (SiGe) BiCMOS process to ensure robust, high-speed data transmission, delivering elevated linearity and ultra-low jitter. The device also supports Modern Standby (S0 Low Power Idle) mode, with power consumption below 5mW in deep standby while maintaining readiness for rapid wake-up.

With four independent differential channels, the PI3EQX32904Q works with any data rate or coding style without interfering with link setup, making it suitable for evolving automotive interface standards. The device integrates programmable linear equalization, output linearity, and flat gain control via I2C. This capability allows designers to optimize signal performance across a wide range of physical media and system configurations without requiring extensive firmware support. The flexibility to extend PCB trace lengths helps reduce intersymbol interference, minimizing cost and power consumption.

The PI3EQX32904Q operates from a 3.3V supply across a -40°C to +85°C temperature range. The device is available in a W-QFN3063-46 (ZR46) package and priced from $4.84 in 1,000-piece quantities.

Diodes Incorporated invites attendees of the PCI-SIG® Developers Conference in Santa Clara, California, to visit Booth 12 and engage with its technical experts.

For more information about how ReDrivers can help boost signal quality of high-speed interfaces, please visit: https://www.diodes.com/products/connectivity/signal-integrity-redriversrepeaterssignal-conditioners#.

PCI-SIG® Developers Conference
May 6-7, 2026
Booth 12, Mission City Ballroom
Santa Clara Convention Center
Santa Clara, California, USA

About Diodes Incorporated

Diodes Incorporated (Nasdaq: DIOD), delivers high-quality semiconductor products to the world’s leading companies in the automotive, industrial, computing, consumer electronics, and communications markets. We leverage our expanded product portfolio of analog and power solutions combined with a flexible hybrid manufacturing model that meet customers’ needs. Our broad range of application-specific products, delivered through a total solutions sales approach and supported by global operations including engineering, testing, manufacturing, and customer service, enable us to be a premier provider for high-growth markets. For more information, visit www.diodes.com.

About PCI-SIG

PCI-SIG is the consortium that owns and manages PCI specifications as open industry standards. The organization defines industry standard I/O (input/output) specifications consistent with the needs of its members. Currently, PCI-SIG is comprised of 1,000 industry-leading member companies. To join PCI-SIG, and for a list of the Board of Directors, visit www.pcisig.com.

PCI-SIG, PCI Express, and PCIe are trademarks or registered trademarks of PCI-SIG.

*Automotive-compliant - AEC qualified, manufactured in facilities certified to IATF 16949, supporting PPAP documents.

ReDriver™ is a trademark of Diodes Incorporated.

The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.

All other trademarks are the property of their respective owners.

© 2026 Diodes Incorporated. All Rights Reserved.

Company Contact:
Gurmeet Dhaliwal
Vice President, Corporate Marketing & Investor Relations
Diodes Incorporated
+1 408-232-9003
Contact Us

Source: Diodes Incorporated (P)