Diodes Menu Close

Press Releases

Press Release

Back to Press Room

PCI Express 3.0 Packet Switch From Diodes Incorporated Offers Design Flexibility and Advanced Power Management

Oct 20, 2021

PLANO, Texas--(BUSINESS WIRE)--Oct. 20, 2021-- Diodes Incorporated (Nasdaq: DIOD) has announced the PI7C9X3G816GP, a PCIe® 3.0 packet switch that supports 16-lane operation in flexible 2-port, 3-port, 4-port, 5-port, and 8-port configurations. Designed to meet advanced performance needs, this switch is well-suited for networking and telecommunications infrastructure, security systems, fail-over systems, AI and deep learning, NAS, HBA cards, and data center applications. The wide operating temperature range of -40°C to +85°C also benefits a growing number of industrial applications, such as embedded, industrial PC (IPC) and industrial control.

Proprietary architecture employed in the PI7C9X3G816GP packet switch allows for enhanced flexibility and performance. It can be configured to have multiple port/lane width combinations, such as upstream, downstream, and cross-domain end-point (CDEP), to support fan-out and dual-host connectivity.

Unique to the industry is the integrated PCIe 3.0 clock buffer, which reduces the overall component count, eases product design-in, and helps to reduce bill-of-materials (BOM) cost. The PI7C9X3G816GP supports three reference clock structures: common, separate reference no spread (SRNS), and separate reference independent spread (SRIS). Multiple direct memory access (DMA) channels are embedded into the switch to facilitate efficient communication between the host (or hosts) and connected end-points.

Additional features such as error handling, advanced error reporting, end-to-end data protection with error correction, hotplug, and surprise removal provide enhanced reliability, availability, and serviceability (RAS). In addition, the built-in thermal sensor reports operational temperature instantly. Advanced power management means that the PI7C9X3G816GP aligns with the most stringent energy-saving requirements for building greener data centers. For instance, the packet switch supports seven power states to efficiently align with the power requirements and any inactive hot-pluggable ports are kept in a low-power state. Advanced diagnostic software tools, including PHY Eye™, MAC Viewer™ (embedded LA), and PCIBUDDY™, assist designers throughout system development.

Diodes Incorporated’s PI7C9X3G816GP is supplied in a high-performance flip-chip (HFC) package, with 324-ball BGA format and 19mm x 19mm dimensions. This packet switch has a unit price of $31.00 in 1,000 piece quantities.

PCI Express® and PCIe® are trademarks or registered trademarks and/or service marks of PCI-SIG Corporation.

All product names, logos, brands, trademarks and registered trademarks are property of their respective owners.

About Diodes Incorporated

Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the consumer electronics, computing, communications, industrial, and automotive markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 31 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information visit www.Diodes.com.

Company Contact:
Diodes Incorporated
Emily Yang
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us

Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com

Source: Diodes Incorporated (P)