Press Release
Back to Press Room
PCIe® 7.0 Clock Generator from Diodes Incorporated Delivers Sub-30fs Jitter for Next-Gen AI Infrastructure
The PI6CG33A06 generates precise 25MHz and 100MHz reference clocks and achieves an RMS jitter of less than 30 femtoseconds (fs). This is well below the PCIe 7.0 specification maximum requirement of 67fs and represents a significant improvement over the 80fs level defined by the CK440Q specification from Intel®. This ultra-low jitter provides greater design margins, helping engineers manage signal integrity challenges across complex PCB traces and connectors.
The device provides a stable reference clock for 128.0 GT/s PCIe links, meeting the bandwidth demands of 800G and 1.6T networking and advanced AI accelerators. Accurate timing at these speeds is critical to maintaining performance and reliability in data center systems.
The PI6CG33A06 implements Diodes’ proprietary low-power, high-speed current-steering logic (LP-HCSL) technology with integrated termination. This reduces clock-related power consumption by at least 50% compared to traditional HCSL solutions and lowers the thermal footprint in high-density AI server racks. The high level of integration eliminates the need for up to 24 external resistors, reducing BOM cost, simplifying PCB layout, and freeing board space for cooling or additional compute and memory resources.
Each of the six outputs includes an individual output enable (OE) pin, allowing designers to manage power more effectively and control system operation with greater flexibility. The device supports Intel CK440Q-Lite specifications and is designed for use in existing server clock architectures. This enables designers to reuse proven system designs while improving timing performance and overall system margin.
“PCIe 7.0 specification is pushing system performance to new heights, particularly for AI and high-bandwidth data center applications,” said
The PI6CG33A06 is available in a 40-pin, 5mm x 5mm VQFN (ZLF) package, and is priced from
To arrange a meeting at the
PCI-SIG®
Booth 12,
About
About PCI-SIG
PCI-SIG is the consortium that owns and manages PCI specifications as open industry standards. The organization defines industry standard I/O (input/output) specifications consistent with the needs of its members. Currently, PCI-SIG is comprised of 1,000 industry-leading member companies. To join PCI-SIG, and for a list of the Board of Directors, visit www.pcisig.com.
PCI-SIG, PCI Express, and PCIe are trademarks or registered trademarks of PCI-SIG.
The Diodes logo is a registered trademark of
All other trademarks are the property of their respective owners.
© 2026
View source version on businesswire.com: https://www.businesswire.com/news/home/20260506335080/en/
Company Contact:
Vice President, Corporate Marketing & Investor Relations
+1 408-232-9003
Contact Us
Source: