PLANO, Texas--(BUSINESS WIRE)--Apr. 23, 2013-- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today introduced a new family of current-limited power switches offering high current handling in an ultra-small (2mm x 2mm) package. The new power switches enable power density to be increased in the protection of multiple USB3.0 ports used in applications such as set-top boxes, LED TVs and notebook computers. The six new single-channel devices introduced have an on-resistance of only 70mΩ, cover maximum continuous output currents up to 2.5A and are being made available in the miniature footprint U-DFN2020-6 package.
For any applications subject to heavy capacitive loads and a possibility of short circuit, the switches provide a robust port protection solution, comprising reverse-current blocking, over-current, over-temperature, under-voltage lockout and short-circuit protection. All devices also integrate an output discharge function to ensure controlled discharging of the output capacitor. In addition, the switches’ fast short-circuit response time of 2µs prevents any unnecessary system shutdown or restart.
With an input voltage range of 2.7V to 5.5V, all devices are suited for 3.3V and 5V rail systems in a variety of product designs including set-top boxes, LED TVs and notebooks. Supporting a maximum continuous output current of 2.5A, the AP2501 and AP2511 are, respectively, active-low and active-high enabled and are footprint-compatible with the AP2301 and AP2311 devices handling a 2A continuous output current.
The AP2401 and AP2411 are also 2A rated power switches but provide in addition an output latch-off function that responds to an over current excursion, enabling further optimization of fault behaviour management. All six power switches also feature an open-drain, over-current fault flag with a 7ms deglitch time to prevent false reporting.
As well as the U-DFN2020-6 package, the devices are also offered in SO8, MSOP-8/EP and U-DFN3030-8 package options. Ambient operating temperature range is -40ºC to +85ºC. For further information, visit the Company’s website at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, AC-DC converters and controllers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. Diodes’ corporate headquarters, logistics center, and Americas' sales office are located in Plano, Texas. Design, marketing, and engineering centers are located in Plano; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. Diodes’ wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with four manufacturing facilities located in Shanghai, China, and two joint venture facilities located in Chengdu, China, as well as manufacturing facilities located in Neuhaus and Taipei. Additional engineering, sales, warehouse, and logistics offices are located in Fort Worth, Texas; Taipei; Hong Kong; Manchester; Shanghai; Shenzhen, China; Seongnam-si, South Korea; Suwon, South Korea; Tokyo, Japan; and Munich, Germany, with support offices throughout the world. For further information, including SEC filings, visit Diodes’ website at http://www.diodes.com.
Source: Diodes Incorporated
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
972-987-3900
pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
949-224-3874
lsievers@sheltongroup.com