Press Release
Back to Press Room
Precision-Adjustable Current Limit Power Switch from Diodes Incorporated Provides High Levels of Protection to Automotive Subsystems
With a tight accuracy margin of ±7% at high current levels, the AP22653Q’s current limit threshold can be simply set anywhere between 125mA to 1735mA via use of standard value external resistors. The device’s controlled rise and fall times help to mitigate the effect of surges during turn on/off. In addition, its 5μs short circuit response helps avoid situations requiring system shutdown/restart.
The AP22653Q has a 55mΩ (typical) on-resistance, which significantly reduces power loss and voltage drop at high load currents. The reverse-current protection integrated into this device safeguards against reverse currents when peripherals are being externally powered. Overtemperature protection and undervoltage lockout features are also included. An operational temperature range of -40°C to 125°C is supported.
The AP22653Q power switch is qualified to AEC-Q100 Grade 1, is manufactured in IATF 16949 certified facilities, and is PPAP capable. It is supplied in a compact SOT26 package and has a unit cost of
About
View source version on businesswire.com: https://www.businesswire.com/news/home/20210831005039/en/
Company Contact:
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: