Press Release
Back to Press Room
Space-Saving Schottky Rectifiers from Diodes Incorporated Set New Benchmarks in Current Density
Each device can be employed for a variety of different purposes, serving as blocking or reverse-polarity protection diodes, electrical over-stress protection diodes, and free-wheeling diodes. The rectifiers in this series are designed for use in space-constrained applications - such as portable, mobile, and wearable devices, as well as IoT hardware.
Leading the trio, the SDT4U40EP3 is the industry’s smallest 4A trench Schottky rectifier, being the first ever in a 1608 package. It takes 90% less PCB area than competing devices. Its 800A/cm2 current density, also the highest for a trench Schottky in the industry, is due to its patent-pending innovative cathode design and manufacturing processes. The resulting ultra-low forward voltage performance (0.47V typical) minimizes power losses, enabling the design of higher efficiency systems. Furthermore, its superior avalanche capability makes it robust enough to deal with extreme operating conditions, including transient voltages.
The X3-TSN1616-2 packaged SDM5U45EP3 has a 2mm2 footprint, while the 1.28mm2 footprint of the X3-TSN1608-2 packaged SDM4A40EP3 and SDT4U40EP3 enable system designers to maximize board real estate in modern, highly integrated consumer products. These ultra-thin CSPs, with their 0.25mm (typical) profiles, have shortened thermal paths - resulting in greater power dissipation, reducing thermal BOM costs and increasing reliability.
Advance samples are available upon request from: www.diodes.com/about/contact-us/sales-support/
About
The DIODES logo is a registered trademark of
DIODES is a trademark of
View source version on businesswire.com: https://www.businesswire.com/news/home/20220427005034/en/
Company Contact:
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
President
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: