Press Release
Back to Press Room
Space-Saving TVS from Diodes Incorporated Provides Superior ESD and Surge Protection for High-Speed I/Os
While many competing products must make design trade-offs, either having strong surge protection properties or low input capacitance, the D3V3Z1BD2CSP can deliver both benefits simultaneously. Its ultra-low capacitance of 0.3pF (typical) ensures that signal integrity is maintained by not interfering with or impeding high-speed data communication. Its high peak pulse current (10.5A typical) and low clamping voltage (5.3V) safeguards I/O ports and their sensitive electronics from transient voltages. The risk of electrical overstress damage from activities such as frequent hot swapping is therefore avoided. Complying with the IEC61000-4-2 immunity standard, the D3V3Z1BD2CSP provides robust ESD protection against ±20kV air and contact discharges, thereby improving system reliability.
The D3V3Z1BD2CSP can be used to protect I/O interfaces, such as USB Type-C®, DisplayPort™, HDMI™, and SD-Card, carrying high-speed data rates up to 20Gbps. Its broad operating temperature range, from -55˚C to +150˚C, ensures continued protection even in challenging application environments.
The D3V3Z1BD2CSP TVS from Diodes is supplied in an extremely compact DSN0603 wafer-level chip-scale package, that measures just 0.6mm x 0.3mm x 0.3mm. It is available at
About
The Diodes logo is a registered trademark of
All other trademarks are the property of their respective owners.
© 2023
View source version on businesswire.com: https://www.businesswire.com/news/home/20230328005157/en/
Company Contact:
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
President
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: