Diodes Incorporated
Investors

Press Releases

Press Release

Back to Press Room

Output Voltage Detector from Diodes Incorporated Improves Transient Performance of Primary-Side Regulation Systems

Jan 12, 2016

PLANO, Texas--(BUSINESS WIRE)--Jan. 12, 2016-- Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today introduced the AP4341S. This device offers a high-performance and cost-effective solution for power adapters and chargers used in portable and consumer applications. This output voltage detector uses a patented design to address the need for fast transient performance in primary-side regulation systems.

The AP4341S works in conjunction with primary-side regulation controllers, such as Diodes’ AP3776 or AP3785 devices, to monitor the secondary-side voltage and provide a periodic ‘wake-up’ signal to the controller, coupled via the transformer, when that voltage drops below a certain threshold. Fast detection, with a pulse at 33kHz, delivers improved transient performance and greater efficiency, supporting green-mode applications through reduced standby power losses.

Offered in a SOT23 package and requiring no external components, the AP4341S provides a highly cost-effective PSR solution. Further information is available at www.diodes.com.

About Diodes Incorporated

Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes’ products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, AC-DC converters and controllers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. Diodes’ corporate headquarters and Americas’ sales office are located in Plano, Texas. Design, marketing, and engineering centers are located in Plano; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. Diodes’ wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two additional facilities located in Shanghai, China. Diodes has assembly and test facilities located in Shanghai and in Chengdu, China, as well as in Neuhaus and in Taipei. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; Shanghai; Shenzhen, China; Seongnam-si, South Korea; and Munich, Germany, with support offices throughout the world. For further information, including SEC filings, visit Diodes’ website at www.diodes.com.

 

Source: Diodes Incorporated

Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
972-987-3900
pressinquiries@diodes.com
or
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
949-224-3874
lsievers@sheltongroup.com