Press Release
Back to Press Room
High Current, High Accuracy LDO from Diodes Incorporated Addresses Noise-Sensitive Power Conversion Applications
The AP7179D has a ±1% output accuracy across line, load, and temperature. This device’s 180mV (maximum) dropout voltage at a 3A load current supports a wide voltage conversion range. Its low-noise reference and error amplifier enables a minimal noise floor. In addition, its 40dB power supply rejection ratio (PSRR) at 500kHz substantially lowers the coupling of input supply noise to the output.
There are two output voltage selection modes for this LDO: pin-programmable between 0.8V and 3.95V, or adjustable using an external resistor divider from 0.8V to 5.5V. The resulting flexibility significantly reduces the number of accompanying components needed.
The device’s low output noise mitigates both power-supply-generated phase noise and clock jitter. Because of this, alongside its high-current capabilities, this device is compatible with high-performance processors, such as FPGAs, ASICs, and DSPs.
The AP7179D is housed in a compact 20-pin W-QFN3535 (Type A1) package, and it is available at
About
The Diodes logo is a registered trademark of
All other trademarks are the property of their respective owners.
© 2023
View source version on businesswire.com: https://www.businesswire.com/news/home/20230906116981/en/
Director, Investor Relations and Corporate Marketing
+1 408-232-9003
Contact Us
Source: