Press Release
Back to Press Room
Boost/SEPIC Controller from Diodes Incorporated Enables 50kHz LED-Wide PWM Dimming in Automotive Lighting Applications
Automotive headlamp manufacturers can use SEPIC topology to enable high or low beam LED array drivers that operate directly from a vehicle’s battery, instead of using the conventional two-stage topology of a boost followed by a buck converter or a full-bridge buck-boost topology. The SEPIC functionality of the AL8853AQ supports cost-effective, simple buck-boost-like topology, which is well-suited for head-up display systems: an increasingly popular feature in automotive designs.
The wide input range (6V to 40V) of the AL8853AQ supports a typical 12V vehicle battery voltage input. Its 200mV feedback reference voltage has ±3% tolerance to maintain tight brightness control while improving efficiency. The fixed 400kHz switching frequency of the AL8853AQ supports low electromagnetic interference (EMI) by using a fundamental frequency outside the medium wave (MW) band. In addition, this controller’s fast (50kHz) pulse width modulation (PWM) to analog dimming mode (100% down to 1%) prevents visible low or high-frequency flickering usually associated with PWM dimming. The AL8853AQ also includes robust protection features to guard against unexpected overvoltage, overcurrent, overtemperature, and diode and inductor short-circuit events.
The AL8853AQ is qualified to AEC-Q100 Grade 1, manufactured in IATF 16949 certified facilities, and is PPAP capable. This controller is available in a SO-8 package at
About
Automotive-compliant - AEC qualified, manufactured in IATF 16949 certified sites supporting PPAP documents.
The Diodes logo is a registered trademark of
All other trademarks are the property of their respective owners.
© 2023
View source version on businesswire.com: https://www.businesswire.com/news/home/20230912002379/en/
Director, Investor Relations & Corporate Marketing
+1 408-232-9003
Contact Us
Source: