Diodes Incorporated
Investors

Press Releases

Press Release

Back to Press Room

Self-Adapting USB 2.0 Signal Conditioner IC from Diodes Incorporated Saves Power and Simplifies System Design

Apr 25, 2024

PLANO, Texas--(BUSINESS WIRE)--Apr. 25, 2024-- Diodes Incorporated (Diodes) (Nasdaq: DIOD) today announces the introduction of the PI5USB212, a USB 2.0 signal conditioner that operates from a supply voltage down to 2.3V. Designed for use in notebooks, PCs, docking stations, cable extenders, TVs, and monitors, the PI5USB212 automatically detects a USB 2.0 high-speed connection. It also preserves signal integrity when driving long PCB traces or cables of up to 5 meters.

This IC symmetrically boosts the USB D+ and D– channels for common-mode stability and applies pre-emphasis to compensate for intersymbol interference (ISI). The wide supply voltage range simplifies system design and extends the operating window of portable and battery-powered equipment.

The device is configured using either I2C commands or pin strapping, adjusting signal-boost and ISI-compensation levels. It has two control pins (boost/SEN); pulling the boost pin down via different resistors controls the AC gain/pre-emphasis levels. The SEN pin selects high, low, or medium receiver sensitivity (DC gain) to ensure optimum signal integrity, depending on channel conditions. It automatically detects a low-speed (LS) mode/full-speed (FS) connection to avoid applying signal compensation when not needed.

The PI5USB212 is compatible with USB 2.0, OTG 2.0, and battery-charging (BC) 1.2, and supports USB features including device-attach and high-speed detection, as well as a 5.5V tolerance. It automatically detects when no USB attachment is present and saves energy by reducing its supply current to 0.7mA (typical), and 13µA (typical) when disabled via the RSTN disable pin.

The PI5USB212 is supplied in a 12-pin, 1.6mm x 1.6mm, quad flat no-lead (QFN) package, and is available at $2.70 in 3,500-piece quantities.

About Diodes Incorporated

Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the automotive, industrial, computing, consumer electronics, and communications markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 32 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information visit www.diodes.com.

The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.

All other trademarks are the property of their respective owners.

© 2024 Diodes Incorporated. All Rights Reserved.

Gurmeet Dhaliwal
Director, Investor Relations & Corporate Marketing
Diodes Incorporated
+1 408-232-9003
Contact Us

Source: Diodes Incorporated (P)