Press Release
Back to Press Room
10Gbps Automotive-Compliant Crossbar Switch from Diodes Incorporated Simplifies In-Vehicle USB-C Connectivity
The PI3USB31532Q supports three configuration modes with USB Type-C compliance, providing a range of options for designers. It can connect a single lane of USB 3.2 Gen 2 to the USB Type-C connector; connect one lane of USB 3.2 Gen 2 and two channels of DP 2.1 UHBR10; or connect four channels of DP 2.1 UHBR10. When configured for DisplayPort, the PI3USB31532Q also connects the complementary AUX channels to the USB Type-C sideband pins: SBU1 and SBU2. Its configuration is controlled by I2C or on-chip logic using four external pins.
Packaged in the 40-pin W-QFN3060-40 and occupying only 3mm x 6mm, the PI3USB31532Q delivers flexibility and performance with the advantage of a space-saving outline. High signal integrity is assured with its -3dB bandwidth of 8.3GHz, and low insertion loss, return loss, and crosstalk of -1.7dB, -15dB, and -38dB respectively at 10Gbps.
The new crossbar switch is automotive compliant*—qualified to AEC-Q100 Grade 2, allowing use in environments exposed to temperatures from -40°C to +105°C, manufactured in IATF 16949 certified facilities, and is PPAP capable. The PI3USB31532Q is available at
About
The Diodes logo is a registered trademark of
ReDriver™ is a trademark of
All other trademarks are the property of their respective owners.
© 2024
View source version on businesswire.com: https://www.businesswire.com/news/home/20240502639770/en/
Director, Investor Relations & Corporate Marketing
+1 408-232-9003
Contact Us
Source: