Press Release
Back to Press Room
Field-Plated Super Barrier Rectifier® Devices from Diodes Incorporated Deliver Industry-Leading Efficiency and Reliability in Automotive Systems
Unlike conventional Schottky rectifiers, Diodes’ proprietary and patented SBRFP technology employs a metal oxide semiconductor (MOS) manufacturing process that overcomes the limitations of Schottky and PN junction diodes. The SBRFP8A60P5Q delivers the industry’s lowest maximum forward voltage (VF) of 0.55V at 8A, reducing conduction losses and enabling cooler operation in high-current applications. Meanwhile, the SBRFP2M60P1Q and SBRFP3M60SAFQ provide industry-leading IR leakage performance, with maximum currents of 12µA and 7µA, at 25°C and 125°C. These characteristics help improve efficiency while minimizing the risk of thermal runaway under high-temperature operating conditions.
The new devices also offer significantly greater avalanche capability than traditional Schottky rectifiers. Depending on the device, avalanche energy ratings reach up to 145mJ, enabling the rectifiers to withstand surge events, load dumps, and transient conditions commonly encountered in automotive electrical systems. This avalanche capability is five to ten times greater than conventional Schottky rectifiers, improving overall system robustness and reliability.
The SBRFP family is available in various packages, including PowerDI®123 (SBRFP2M60P1Q), PowerDI5 (SBRFP8A60P5Q), and SMAF (SBRFP2M60SAFQ and SBRFP3M60SAFQ). The devices maintain stable operation across a junction temperature range of -55°C to +175°C, making them suitable for harsh automotive environments.
The SBRFP family is available in 1,000-piece quantities at:
SBRFP2M60P1Q
SBRFP8A60P5Q
SBRFP2M60SAFQ
SBRFP3M60SAFQ
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), delivers high-quality semiconductor products to the world’s leading companies in the automotive, industrial, computing, consumer electronics, and communications markets. We leverage our expanded product portfolio of analog and power solutions combined with a flexible hybrid manufacturing model to meet customers’ needs. Our broad range of application-specific products, delivered through a total solutions sales approach and supported by global operations including engineering, testing, manufacturing, and customer service, enable us to be a premier provider for high-growth markets. For more information, visit www.diodes.com.
*Automotive-compliant - AEC qualified, manufactured in facilities certified to IATF 16949, supporting PPAP documents.
The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.
PowerDI® is a registered trademark of Diodes Incorporated.
Super Barrier Rectifier® is a registered trademark of Diodes Incorporated.
All other trademarks are the property of their respective owners.
© 2026 Diodes Incorporated. All Rights Reserved.
View source version on businesswire.com: https://www.businesswire.com/news/home/20260924259970/en/
Company Contact:
Gurmeet Dhaliwal
Vice President, Corporate Marketing & Investor Relations
Diodes Incorporated
+1 408-232-9003
Contact Us
Source: Diodes Incorporated (P)