Press Release
Back to Press Room
Intelligent High-Side Switches from Diodes Incorporated Deliver Combined Protection and Diagnostics to Safely Drive 12V Automotive Loads
Each device features a vertical DMOS N-channel MOSFET and an integrated controller that protects against short circuits, manages inrush currents, and safeguards against overvoltage conditions, including load dumps. In addition, the switches provide overtemperature protection with auto-restart, alongside protection against electrostatic discharge (ESD) damage. Loss of ground and reverse polarity protection can also be implemented with minimal external components. Onboard diagnostics detect fault conditions and self-protection events, including open load, overload, and overtemperature shutdown.
The ZXMS81030SPQ is available in the SO-8EP and the ZXMS82030S14PQ and ZXMS82045S14PQ are available in the SO-14EP package. Both packages feature exposed underside heatsinks and are thermally efficient. The ZXMS81030SPQ is available at
The devices are being exhibited at electronica 2026 on Diodes’ Booth 211 in Hall C6 as part of the company’s 48V power tree demonstration, which showcases technologies for efficient power distribution and load control in evolving automotive power architectures. Within the demo, the IntelliFET is used as a load switch, providing a switched 12V output with its associated protection and diagnostic features.
For more information about the IntelliFET portfolio, please visit: https://www.diodes.com/products/discrete-semiconductors/mosfets/intellifet-products.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), delivers high-quality semiconductor products to the world’s leading companies in the automotive, industrial, computing, consumer electronics, and communications markets. We leverage our expanded product portfolio of analog and power solutions combined with a flexible hybrid manufacturing model to meet customers’ needs. Our broad range of application-specific products, delivered through a total solutions sales approach and supported by global operations including engineering, testing, manufacturing, and customer service, enable us to be a premier provider for high-growth markets. For more information, visit www.diodes.com.
*Automotive-compliant - AEC qualified, manufactured in facilities certified to IATF 16949, supporting PPAP documents.
IntelliFET® is a registered trademark of Diodes Incorporated in the United States and other countries.
The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.
All other trademarks are the property of their respective owners.
© 2026 Diodes Incorporated. All Rights Reserved.
View source version on businesswire.com: https://www.businesswire.com/news/home/20261110119999/en/
Company Contact:
Gurmeet Dhaliwal
Vice President, Corporate Marketing & Investor Relations
Diodes Incorporated
+1 408-232-9003
Contact Us
Source: Diodes Incorporated (P)